Keysight 89600 VSA .NET API
TestModelSetup Class Members
See Also  Properties  Methods 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : TestModelSetup Class

Glossary Item Box

The following tables list the members exposed by TestModelSetup.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorTestModelSetup ConstructorOverloaded.   —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyBandwidthGets or sets the bandwidth used when applying the test model.  —
Public PropertyDuplexSchemeGets or sets the duplex scheme used when applying the test model.  —
Public PropertyIsInterferenceEnabledGets or sets a value indicating whether interference is enabled.  —
Public PropertyIsMapPdschInPdcchSymbolsGets or sets a value indicating whether to map PDSCH in PDCCH in symbols.  —
Public PropertyNumberOfPdschLayersGets or sets the number of PDSCH layers when test model 1.1 is applied.  25.00
Public PropertyNumerologyGets or sets the numerology used when applying the test model.  —
Public PropertySupportedModulationFormatForTM2And31Gets or sets the lower modulation format supported by this UE for test model 2 and test model 3.1 measurement.  25.40
Public PropertyTestModelDeviceTypeGets or sets a value indicating the device type the test model is applied to.  29.40
Public PropertyTestModelNumberGets or sets the test model number used when applying the test model.  —
Public PropertyVersionGets or sets the version used when applying the test model.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodSerialize  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also