Keysight 89600 VSA .NET API
TrackingSignalBasis Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : TrackingSignalBasis Enumeration


Glossary Item Box

Enum values indicating what portions of the demodulated signal are used to generate symbol tracking estimates.

Syntax

Visual Basic (Declaration) 
Public Enum TrackingSignalBasis 
   Inherits System.Enum
C# 
public enum TrackingSignalBasis : System.Enum 
C++/CLI 
public enum class TrackingSignalBasis : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Mode3GppTracking following 3GPP conformance test specification25.20
RSTracking from RS—
RSAndDataTracking from RS+Data—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also