Keysight 89600 VSA .NET API
VrbToPrbInterleaverSize Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : VrbToPrbInterleaverSize Enumeration


Glossary Item Box

Specifies the interleaver size configurable between 2 and 4 PRBs for PDSCH

Syntax

Visual Basic (Declaration) 
Public Enum VrbToPrbInterleaverSize 
   Inherits System.Enum
C# 
public enum VrbToPrbInterleaverSize : System.Enum 
C++/CLI 
public enum class VrbToPrbInterleaverSize : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
N2The interleaver size is 2 PRBs.—
N4The interleaver size is 4 PRBs.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.00

See Also