Error Codes

The 89600 VSA SCPI interface logs errors to the system error log (SYST:ERR? query). The following table lists the possible error codes for the 89600 VSA SCPI interface, their numerical codes, and the reason for the error.

-113 UndefinedHeader Unknown command.
-102 SyntaxError SCPI arguments not in the proper format.
100 UnhandledException An unhandled exception occurred when accessing the 89600 VSA .NET interface (SCPI commands are translated to .NET API calls).
130 ConnectionError Error when trying to connect to the 89600 VSA application.
140 ObjectNotFound Could not find a type in the 89600 VSA .NET API. Typically used when a .NET Enum could not be found that matched the enum name specified as a string argument of a SCPI command.
150 NotValidForCurrentConfig A command could not be executed due to the current state of the 89600 VSA application.
160 InvalidArgument SCPI command arguments are invalid.
161 InvalidUnits Units specified for SCPI command argument are invalid.
162 InvalidIndex Index specified in SCPI command argument is invalid.
200 Deprecated Indicates that something in a command or query has been deprecated.