MATLAB Example Program
An example Visual Studio Project written in C# is located in the %PROGRAMFILES%\Agilent\89600 Software 20xx\89600 VSA Software\Examples\SCPI\Matlab\ folder that demonstrates the following concepts:
- Connecting and disconnecting the SCPI session with basic exception handling
- Setting the instrument timeout period
- Presetting the VSA application and measurement
- Checking to see if the VSA application is running and how to start the VSA if it is not running
- Starting a measurement and waiting for operation complete
- Querying trace data in ASCII and binary data formats