About Error Summary Data (802.16 OFDM)
The Error Summary results are shown in the upper section of the Syms/Errs trace display. This topic contains the following measurement, analysis, and programming information:
- Available Error Summary Data
- Averaging and Error Summary Data
- Using Band Power markers to limit Error Information
- Querying summary table data results programmatically
Available Error Summary Data
A list of the available error data is provided in the Available Error Summary Data topic which also links to detailed descriptions for each error result.
Averaging and Error Summary Data
When averaging is on, averaging is applied to the numeric error data in the symbol/errors table, see Averaging with Digital Demodulation. Error data from the current scan is not included in the average if any of these conditions exist:
- Pulse Not Found
- Sync Not Found
- Carrier Unlock.
- DATA?
- Pulse too Short
For more information, see Troubleshooting and Trace Indicators help.
Using Band Power markers to limit Error Information
For RCE Relative Constellation Error is the RMS level of the Error Vector Magnitude, averaged over all subcarriers and all detected OFDM symbols. (EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format.) error information for all points over a selected region, use the band-power markers with the and trace data. The trace data will compute the RCE (EVM) for all symbols within a specified subcarrier region and trace data will compute the RCE (EVM) for all subcarriers within a specified symbol-time region.
For example, here's how the symbol RCE (EVM) for OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. subcarriers 11, 12, and 13 could be computed. Click to display the trace data; then click and select the check box to turn on the band-power markers.
Now position the band-power markers to select the region of interest; place the markers so that they are exactly on or close to the specific subcarriers of interest. Center the marker at subcarrier 12, enter 12 in the text box and set the width to two carriers, enter 2 in the text box. This encloses the region of interest (subcarriers 11, 12, and 13). Then set Calculate: to to display the RCE (EVM) in %rms, this is the RCE (EVM) (%rms) for all symbols within subcarriers 11, 12, and 13.
The same procedure can be used with the trace data display to find the RCE (EVM) (%rms) for all subcarriers within a specific range of symbol-times.
Querying summary table data results programmatically
To programmatically query the Trace Summary Table data results using the Summary() and SummaryUnit() methods in the MeasurementData object.
See the How To Query Summary Table Data Results topic for more information.
See Also
Syms/Errs trace data (802.16 OFDM)