Manual - Result Length (802.16 OFDM)
            
            : See 802.16 OFDM Standard Setups/Presets Table.
When the check box is selected, the measurement result length can be entered in symbol-times. The VSA ignores the input burst symbol length and uses the symbol length. The VSA will use this value even if it is longer than the measured signals burst length.
See Result Length Parameters for more information about how the VSA determines the measurement result length in , , and modes.
does not limit the result length to the number of symbols transmitted within the burst as is done in mode. The VSA will demodulate the total number of symbols specified by , which if longer than the burst, could lead to unexpected and incorrect data results.
See Also
Result Length Parameters (802.16 OFDM)