Preset to Standard (802.16 OFDMA)
configures the VSA to demodulate and measure a particular OFDMA signal that conforms to a profile of the IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.16e OFDMA standard specification. will configure the Standard, Nominal BW, and Downlink Frame Ratio parameters to match the specified profile and will also reset all other OFDMA parameters to a default state, as described in Using a Standard Setup topic.
The Standard control only configures the demodulator and not the measurement configuration parameters.
To use this feature, select the IEEE 802.16 OFDMA demodulator, select the Subframe Type ( or ) and click the command button and select a preset configuration from the list.
See Also