Bursts in Selected Zone (802.16 OFDMA)

Menu Path: Analysis > IEEE 802.16 OFDMA Demod Properties > Zone Definition tab

Burst in Selected Zone is used to create and edit bursts in a selected zone.

Avaliable parameters are:

See Also

Zone Definition Tab (802.16 OFDMA)