DataRCE Pk (802.16 OFDMA)
DataRCE Pk (%) is the peak EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. value used to calculate the DataRCE result. The number of the symbol that the peak EVM occurred is also provided, this is the "pk at sym" number.
DataRCE Pk at sym is the OFDMA symbol number where the Peak Error Vector Magnitude was detected for the DataRCE Pk result, see DataRCE Pk.
See Also