Time Offset (802.16 OFDMA)
Time Offset is the amount of time (in seconds) between the trigger event used for the measurement and the start of the analyzed OFDMA frame. Time Offset is most useful if external triggering is used to provide a time reference for the measurement relative to an external event. This may be useful for measuring system delay times between different stages of processing.
See Also