Noise Correction Spectrum (Spectral Emissions Mask)
is the measured noise correction trace that will be applied when Noise Correction is turned on.
Noise correction may affect measurement speed. See Noise Correction for more information.
This trace is only available if using Time Domain Input for the Power Spectrum Measurement.
See Also