Raw Main Time (Spectral Emissions Mask)
shows the raw time data read from the input hardware or playback file.
This trace is only available if using Time Domain Input for the Power Spectrum Measurement.
Characteristics of this trace:
- The data has not had instrument calibration corrections applied, so the trace shows a "CAL?" trace message.
- The data has not gone through the VSA's software resampling filters, so is generally not sampled at the specified sample rate.
- The zero time point is where the instrument or the recording actually triggered.
See Also