About Advanced-Radar/Hopping Analysis

Menu Path: Analysis > Type > Radar Analysis > Advanced-Radar/Hopping

The 89600 VSA Advanced-Radar/Hopping Analysis solution (89601BHQC) provides easy-to-use, time-oriented measurements of diverse signal types: Pulsed vs. Continuous Wave (CW) and RF Radio Frequency: A generic term for radio-based technologies, operating between the Low Frequency range (30k Hz) and the Extra High Frequency range (300 GHz). vs. Microwave. It features multiple use cases and workflows tailored for vastly different signal descriptions. For radar (amplitude) pulsed signals, this tool will automatically find pulse edges in time, and then measure metrics such as rise time, fall time, pulse width, PRI (interval), PRF pseudo-random function, duty cycle, peak-to-average ratio and much more. For signals where the power amplitude is constant, this tool can automatically find time regions of constant phase, frequency, or linear chirp rate, and provide relevant metrics. Lastly, for signals that are modulated by regions of constant phase, frequency or linear chirp rate but bursted (i.e. pulsed), this tool can automatically discriminate unique pulses and provide relevant metrics. This allows for analysis of complex signal combinations previously not easily analyzed, such as a bursted (i.e. pulsed) FMCW signal.

Algorithms determine pulse and region characteristics according to methods from IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org. Visit the IEEE at http://www.ieee.org standard 181 for more information.

The Advanced-Radar/Hopping Measurement software also includes the following:

Similar to most VSA measurement extensions, the Advanced-Radar/Hopping Measurement supports data acquisition from all 89600 VSA supported front-end hardware instruments. The user must consider the RF frequency, signal bandwidth and the memory limitations of PC running the VSA. Signals being analyzed may also come from an external down-converter, in which case the 89600 VSA software’s external down-converter feature can be used to ensure that the User Interface and results have correct frequency labeling.

See Also

Advanced-Radar/Hopping Measurement Properties Dialog Box

Result Tables

Available Trace Data