Internal Buffer Length (Advanced-Radar/Hopping)

Menu Path: Analysis > Advanced-Radar/Hopping Measurement Properties > Analysis > Statistics Panel

Internal Buffer Length determines the maximum accumulated Trend and Histogram statistical data set size.

When the current accumulated statistical data set size exceeds the specified Internal Buffer Length points, only the most recently accumulated Internal Buffer Length number of points is retained within the accumulated Trend and Histogram statistical data set.