Segmented Capture (Advanced-Radar/Hopping)

Menu Path: Analysis > Advanced-Radar/Hopping Measurement Properties > Capture

Specifies if the capture, detection and analysis are performed over a single continuous time acquisition or instead over multiple time acquisition segments.

When Segmented Capture mode is enabled, the Acquisition Length property is grayed-out (unavailable) since user should specify desired Segmented Capture mode acquisition length using the separate Segment Length (s) and Segment Count properties.

Segmented Capture mode can also be enabled in the Acquisition > Segmented Capture tab.

When Segmented Capture mode is enabled:

The input acquisition segment identifier associated with each detected pulse is reported as the Segment metric within the Pulse Table results.

See Also

Segmented Data Acquisition