Minimum Width (Advanced-Radar/Hopping)

Menu Path: Analysis > Advanced-Radar/Hopping Measurement Properties > Detection

When the Minimum Width checkbox is enabled, you can specify the minimum pulse width time, in seconds, to be considered valid for the purpose of pulse detection. Any measured pulse width durations less than the specified time value will be considered invalid, and excluded from the pulse analysis results.

For the Minimum Width and Maximum Width parameters, the width of the pulse is defined as the time between the pulse-on and pulse-off transitions (see Hysteresis topic). The Pulse Width reported in the pulse table is computed using the Pulse Width Threshold and thus can vary slightly from the Minimum/Maximum Width values.

When the Minimum Width checkbox is disabled, no minimum pulse width time validation checks are applied.