Amplitude Meas Time (Advanced-Radar/Hopping)
Menu Path:
Amplitude Meas Time reports region-synchronized measured signal amplitude level samples over time in the units determined by Trace Y Scale and Trace Format selection combination.
The Inst Amplitude Meas Time is a non-averaged version of Amplitude Meas Time .
The Y Scale units of the reported Amplitude trace can be configured from either the Trace menu, as shown below, or by right clicking the Y Scale trace area (located to the left of a trace grid).
By selecting appropriate Y Unit and trace Format selection combination as listed below you can display Amplitude Meas Time trace results in either dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer, Watt or Volt units:
- Y Unit = Auto: Format = Log Mag
- dBvPk units
- Y Unit = Auto: Format = Linear Mag
- Volt units
- Y Unit = Auto: Format = Real
- Volt units
Valid trace Format selections are:
- Log Mag (dB)
- Linear Mag
- Real
The Ripple Analysis Width is displayed as a dark green band that is centered on each pulse.