Auto Correlation (Trace Data)
shows the auto correlation for the selected input channel. Auto correlation is a form of correlation, a measure of the similarity between two signals.
The Auto Correlation trace is not supported with Segmented Capture. If this trace is open while Segmented Capture is enabled, the NO DATA indicator will appear on the trace.
For further details, see Auto Correlation for Vector Measurements.