Acquisition Spectrum (Advanced-Radar/Hopping)
The trace consumes the Frequency vs. Time input parameters to create an RMS Spectrum. This trace does the same thing as the Freq v Time Heatmap, but instead of stacking the time blocks/slices together, it takes the average of these blocks/slices to achieve an RMS Spectrum. The RMS notation at the top of the Trace indicates how many FFTs were included in the RMS Spectrum.
See Also