About Bluetooth Modulation Analysis

The Bluetooth extension (89601BLTC) for the 89600 VSA software demodulates and analyzes Bluetooth transmitter signals. The option adds two measurement types:

The two measurements share a common Bluetooth Mode configuration (PHY family, PHY rate, packet type, and channel index) that appears above the tabs in each measurement's properties dialog box.

Bluetooth Demod covers the following transmitter test purposes for the LE PHYs (LE 1M, LE 2M, and LE Coded):

Test

Standard reference

Output power

Core Spec Vol 6, Part A, §3.1.2

Modulation characteristics (Δf1, Δf2)

Core Spec Vol 6, Part A, §3.1.1; RF-PHY Test Spec §4.6.3

Carrier frequency offset and drift (ICFT, drift, drift rate)

Core Spec Vol 6, Part A, §3.1.2; RF-PHY Test Spec §4.6.4

 

Results are reported per burst in the Results Table, with pass/fail limits resolved automatically for the active PHY and packet type and reported in the Limits Table.

The Bluetooth Demod measurement is introduced in this release as a beta feature and supports Bluetooth low energy (LE) signals only.

See Also

Selecting Bluetooth Demod

Bluetooth Demod Properties Dialog Box

Available Trace Data

Troubleshooting Bluetooth Measurements