Limits Table (Bluetooth)

The Limits Table trace shows, for each result in the Results Table, the limit that applies and the resulting pass/fail status. The results run down the rows — the same results in the same order as the Results Table — and the Limit and Status columns run across.

The limits are resolved automatically from the Bluetooth Core Specification for the active PHY Physical Layer rate and packet type — there is no user limit editor.

Limit Column

The limit is shown in whichever form the specification defines for that result:

The Df2 Rate limit carries additional context, because its bound is a percentage while the deviation floor those percentages are measured against depends on the PHY. It reads >= 99.90 % @ 185.0k on LE 1M and >= 99.90 % @ 370.0k on LE 2M, so the criterion that actually moved with the PHY stays visible.

Status Column

Two different situations produce ***, and the Results Table distinguishes them. Read across to that result's Value cell:

A result that has no limit is never reported as PASS; it reads *** instead.

Results With No Limit

Which results show a blank Limit cell depends on the active PHY rate and packet type; it is not a fixed list. For example:

See Also

Results Table

Burst Table

Available Trace Data