Time (Bluetooth)

The Time trace shows the time record before demodulation, as shown in the following block diagram. For Bluetooth Demod, this is the time record of the analyzed burst.

image\blk_time_wmf.jpg

For the time traces (Time, Search Time, and Raw Main Time), 0 sec on the X-axis is the trigger location.

The Time trace is unaffected by time averaging.

Marker Coupling

When marker coupling is used, markers on applicable Demod traces (e.g., Err Vect Time, IQ Meas Time, IQ Ref Time, Mag Error, Phase Error) will couple to the corresponding point on the Time, Search Time and Raw Main Time traces. For Demod traces, frame start (symbol 0) = 0 sec on the x-axis.