Comp Error Vector Time (cdma2000/1xEV-DV)
When cdma200/1xEV-DO demodulation is enabled, the trace is the error-vector, time-domain data for the composite signal.
The trace data is computed from the first PCG in the measurement and the and parameter settings are ignored (see Measurement Interval and Offset).
Concept Information
This trace data is identical to the trace data except that the source data is the composite signal. See Chan Error Vector Time for concept information.
See Also