Spectrum (cdma2000/1xEV-DV)
trace is the frequency spectrum of the pre-demodulated trace data. The data is Windowed and FFTed to create the Spectrum display.
If averaging is on, Spectrum trace data is the averaged Instantaneous Spectrum trace data. When averaging is set to zero, the Spectrum trace data is equal to the Inst Spectrum trace data.
VSA signal flow (see Digital Demodulation Block Diagram):

See Also