Samples/Symbol (Channel Sounding)
specifies the number of samples per symbol to use when calculating impulse response and affects other metrics such as symbol clock error estimation.
The input signal is resampled from the current sample rate (determined by VSA Span) to Samples/Symbol * (Symbol Rate * (1+Timing Adjust/1E6)).
2, 4, 8
2
See Also