Sequence Length (Channel Sounding)
selects the base length of the sounding sequence. The length of a repetition of the sounding signal is 8 * base length. Max delay spread is 2x the sequence length.
32 Symbols; 64 Symbols; 128 Symbols; 256 Symbols; 512 Symbols; 1,024 Symbols; 2,048 Symbols; 4,096 Symbols; 8,192 Symbols; 16,384 Symbols; 32,768 Symbols, 65,536 Symbols
128 Symbols
See Also