CDF (Channel Sounding)
The trace data displays the cumulative distribution function (CDF Cumulative Distribution Function: The cumulative probability that a parameter will be less than a given value X.) for the selected input channel. CDF is computed by integrating the PDF 1) Probability Density Function Trace Data, or 2) Portable Document Format (PDF) created by Adobe Systems is an open standard for document exchange. (Probability Density Function). CDF is explained in online help for the CCDF trace data.
See Also