Signal Power (dBm) (Channel Sounding)
is an estimate of the power of the sounding signal, calculated from the current impulse response, and is expressed in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer. This value is calculated after the measurement filter has been applied.
See Also