Clock Error (Component Test)
shows the estimated deviation between the stimulus signal clock (derived from the stimulus definition) and the measured stimulus signal, in units of parts per million (ppm). This result is provided for each measurement channel.
Clock offset between stimulus and measurement hardware can be compensated using the Timing Adjust parameter.
See Also