Include Unbalanced in EVM Equalization (Component Test)
When is enabled, the equalized EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. model includes the unbalanced (for homodyne I+jQ systems that measure I and Q separately) term of the channel. When cleared, only the balanced term is used.
Default: Enabled (checked)
See Also