Coherence Unbal (Component Test)
is the coherence that is due to IQ impairments. In other words, it is the coherence between the output and the conjugate, frequency-mirrored version of the input (which will be zero if there are no IQ impairments).
The non-averaged unbalanced coherence is shown in the Inst Coherence Unbal trace.
See Also