Frequency Response (Component Test)

Frequency Response trace data is a two-channel measurement defined as the output of a device-under-test (DUT Device under Test: An acronym used to describe some type of electrical apparatus connected to test instrumentation. The apparatus can range from a single component to a complex subsystem such as a mobile phone, base station or MSC.) divided by its input (make sure channel M is connected to the input of your DUT and channel N is connected to its output).

This trace data is available only when more than a single input channel is selected.

The exact computation used for frequency response depends on the type of average used:

If the average is:

the VSA uses this formula:

None

A

Time

A

Time exponential

A

rms

B

rms exponential

B

peak hold/continuous peak hold

Frequency response is unavailable

 

Formulas:

A: (linspec,N) / (linspec,M)

B: (cross spectrum) / (power spectrum Ch M)

Term

Definition

linspec,N

linear spectrum channel N