Inst Ch Frequency Response (Component Test)
is the non-averaged channel frequency response. If averaging is enabled, this trace does not show the effects of averaging.
For information about channel frequency response, see Ch Frequency Response.
I and Q Inst Channel Frequency Response Traces
There are also traces for I and Q that express the instantaneous frequency response separately for the In Phase and Quadrature Phase components of the channel. These traces are computed from the Balanced and Unbalanced responses.
See Also