Inst Ch Impulse Response (Component Test)

Inst Ch Impulse Response (Balanced) is the non-averaged channel impulse response. If averaging is enabled, this trace does not show the effects of averaging.

For information about channel impulse response, see Ch Impulse Response.

I and Q Inst Channel Impulse Response Traces

There are also traces for I and Q that express the instantaneous impulse response separately for the In Phase and Quadrature Phase components of the channel. These traces are computed from the Balanced and Unbalanced responses.

See Also

Available Trace Data