Inst Inv Ch Frequency Response (Component Test)
is the non-averaged, inverse channel frequency response. If averaging is enabled, this trace does not show the effects of averaging.
For information about inverse channel frequency response, see Inv Ch Frequency Response.
I and Q Inst Inv Channel Frequency Response Traces
There are also traces for I and Q that express the instantaneous inverse frequency response separately for the In Phase and Quadrature Phase components of the channel. These traces are computed from the Balanced and Unbalanced responses.
See Also