Inst Inv Ch Impulse Response (Component Test)
is the non-averaged, inverse channel impulse response. If averaging is enabled, this trace does not show the effects of averaging.
For information about inverse channel impulse response, see Inv Ch Impulse Response.
I and Q Inst Inv Channel Impulse Response Traces
There are also traces for I and Q that express the instantaneous inverse impulse response separately for the In Phase and Quadrature Phase components of the channel. These traces are computed from the Balanced and Unbalanced responses.
See Also