Inv Ch Impulse Response Unbal (Component Test)
is the unbalanced part of the inverse channel impulse response. Unbalanced inverse channel impulse response is calculated for each measurement channel and is averaged over the number of repetitions of the stimulus signal specified by the Analysis Interval.
The x-axis of this trace is in units of seconds. The impulse response traces show the supported delay spread.
To increase the available delay spread range, increase the number of tones while decreasing the Tone Spacing to maintain the same ratio (same stimulus bandwidth).
When RMS or RMS Exponential averaging is enabled, this trace will show the averaged unbalanced channel impulse response.
The non-averaged unbalanced inverse channel impulse response is shown in the Inst Inv Ch Impulse Response Unbal trace.
See Also