Tracking Response (Component Test)

The X-axis of the Tracking Response trace is time, with t=0 matching the start of the Analysis Interval, and length matching the Analysis Interval. The unitless complex values represent the phase and gain drift estimated on the measured signal. Using different coordinate transforms of this trace help isolate signal drift characteristics like phase, amplitude, or frequency (using Group Delay coordinate transform).

See Also

Available Trace Data

Timing Adjust