Gain Imb (Custom IQ)

Gain Imb (IQ Gain Imbalance) compares the gain of the I signal with the gain of the Q signal, as follows:

 image\IQGainImb_wmf.jpg

The effects of IQ gain imbalance are best viewed in constellation diagrams where the width of the constellation diagram is different than its height.

Gain imbalance may be a positive or negative value because it is expressed as a logarithmic value. The gain imbalance is always positive if averaging is ON and Pattern Search is OFF.

For non-rectangular formats (such as 8-PSK Phase Shift Keying: A broad classification of modulation techniques where the information to be transmitted is contained in the phase of the carrier wave.), IQ Gain Imbalance may look like Quadrature Skew, and vice-versa. This occurs when the VSA is phase locked to an orientation that is different than that of the modulator.

See Also

IQ Gain Imbalance and Quadrature Skew Parameter Interaction (Custom IQ)

Quad Err (Custom IQ)