Gaussian Filter (Custom IQ)
The filter is typically used for MSK Minimum Shift Keying and FSK Frequency Shift Keying: A form of modulation using multiple carrier frequencies to carry the digital information. The most common is the two frequency FSK system using the two frequencies to carry the binary ones and zeros. signals. Typically MSK transmission performs all filtering in the transmitter (where T is the symbol interval).

See Also