Reset Equalizer (Custom IQ)
The VSA defines the to have a unit impulse response when equalization is first turned on. If is selected, the VSA then reshapes the after each subsequent measurement. Click the button at any time to reset the equalization filter to a unit impulse response. There are several conditions that automatically reset the . For details, see Filter Coefficients in About Adaptive Equalization.
This button is available only when the Equalization Enable check box is selected.
Large values may cause the adaptation algorithm to become unstable. If this happens, reduce the by clicking to reset the filter; then resume the measurement.
See Also