Constellation (Custom IQ)
displays the name of the currently configured constellation.
If a Quick Setup is selected, the name of the Quick Setup will appear in the Constellation field.
If a constellation was created or edited using the Constellation Editor, the name of the saved constellation will appear in this field.
See Also