Demod Bits (Custom IQ)
The trace is similar to the lower section of the Syms/Errs trace, but it shows an extended view of the binary bits for each symbol. The first bit in the table corresponds to the first bit of the first symbol.
See Also
The trace is similar to the lower section of the Syms/Errs trace, but it shows an extended view of the binary bits for each symbol. The first bit in the table corresponds to the first bit of the first symbol.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |