Eq Impulse Response (Custom IQ)
When is enabled and the equalizer is ON, the trace shows the impulse response of the equalization filter.
The VSA applies the equalization filter to the measurement when the check box is selected. When the check box is cleared, the filter still exists but is not applied to the signal. The filter may be turned on and off without resetting the filter coefficients.
For complete details, see Equalization Enable.