Error Vector Spec (Custom IQ)
When is enabled, the trace shows the spectrum of the Error Vector Time trace. In other words, the VSA derives the trace and then windows and FFTs this trace to produce the trace.
The custom IQ demodulator removes carrier frequency error. Therefore, in the error vector spectrum display, you must add the carrier frequency error to marker readouts to obtain exact frequency information. The carrier frequency error () is shown in the symbol table.
The center frequency and span for the trace is identical to the IQ Meas Spec.