Inst IQ Ref Spec (Custom IQ)
When is enabled, is the instantaneous spectrum of the IQ Ref Time trace. In other words, is the non-averaged versions of IQ Ref Spec trace data.
The custom IQ demodulator removes carrier frequency error. Therefore, in the error vector spectrum display, you must add the carrier frequency error to marker readouts to obtain exact frequency information. The carrier frequency error () is shown in the symbol table.
See Also