FreqErr (Custom OFDM)
parameter is the carrier frequency error relative to the measurement hardware's center frequency. This parameter is displayed in Hertz and is the amount of frequency shift, from the measurement hardware's center frequency, that the VSA must perform to achieve carrier lock.
Errors in RF Radio Frequency: A generic term for radio-based technologies, operating between the Low Frequency range (30k Hz) and the Extra High Frequency range (300 GHz). frequency, LO frequency, or digitizer clock rate could all be contained in the carrier frequency error.
See Also
Available Error Summary Results