Time Offset (Custom OFDM)
is the offset to the analysis start boundary (frame start) and is expressed relative to the trigger t=0 point when Trigger Delay = 0 sec. When Trigger Delay is non-zero, then Trigger Delay will be subtracted from the TimeOffset value.
The time offset will not exceed the analysis boundary period length (any integer multiple of the analysis boundary period will be subtracted from the TimeOffset).
See Also
Available Error Summary Results