Inst Ch Frequency Response (Custom OFDM)
The trace is the non-averaged Ch Frequency Response trace data for the specified spatial stream (MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas.) and measurement hardware input channel X (where X is the number of the channel). If averaging is selected, the Inst Ch Frequency Response does not show the effects of averaging.
For information about Ch Frequency Response, see Ch Frequency Response.
See Also